RF Amplifier input port DC part issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RF Amplifier input port DC part issue

962 Views
coyoo
Contributor I

Hello Guys

We are testing the RF Amp part in our application. The part number are BGA2851. Before the input signal is fed into BGA2851, one AC coupling capacitor inserted to cut the input signal's DC part. However, there always exists around 800mV level DC part when we measure BGA2851 input port thru oscilloscope. So we don't know why this can happen? and where does this DC part come from? As following image, the DC level is 840mV.

tek00016.png

Tags (1)
0 Kudos
Reply
2 Replies

945 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

The device internally sets a DC bias point at its input to ensure proper operation of the active transistor. While a coupling capacitor is used to block any DC component from your signal source, the amplifier itself applies a DC voltage at its input terminal.

This behavior is expected and should not pose any issue in normal operation.

0 Kudos
Reply

904 Views
coyoo
Contributor I

Hi ErikaC,

 

Thanks for you reply.

I have several questions need you help:

1. What's the internal bias DC level? Why datasheet does present this character?

2. Do this kind of RF amplifiers amplify the DC part of the input port? If so, in our case, the 840mV DC part will be amplifiered to 8400mV on output port. I thinks this is impossible.

3. BTW, do we need to install inductor after BGA2851's output port?

0 Kudos
Reply