Quick charge 2/3/4.0+

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Quick charge 2/3/4.0+

2,534 Views
hoangdaive
Contributor II

Dear All,

Currently, I'm designing a power adapter as below:

- Power: 18W - 20W

- 1 USB-Type C port (Support QC4+)

- 1 USB-Type A port (Support QC 2, 3)

I'm using your chipset (TEA19051). But i don't understand how to design this product have two output (1 USB-Type C and 1 USB-Type A) that using one chipset (TEA19051).

Can you help me?

4 Replies

2,296 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

You need two outputs with one TEA19051,right?

Sorry that can you tell us where you find some information about one TEA19051 support two channels outputs? I want to make sure I didn't miss something.

2,296 Views
hoangdaive
Contributor II

Hi,

Thanks for your reply!

I see in the datasheet have some information as below:

Support:

- USB Type-C v.1.3

- USB Power Delivery (USB-PD) 2.0 and 3.0 including Programmable Power Supply
(PPS)

- Supports Qualcomm® QuickCharge™ QC2.0, QC3.0, and QC4+ protocols

- Battery Charging 1.2 (BC 1.2)

So, I want to designing a product that support two channels outputs!

0 Kudos
Reply

2,296 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

Yes,it can support such topology but only can support one channel output.

2,296 Views
hoangdaive
Contributor II

Hi,

Yes, thank you so much!

0 Kudos
Reply