Quick charge 2/3/4.0+

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Quick charge 2/3/4.0+

2,531件の閲覧回数
hoangdaive
Contributor II

Dear All,

Currently, I'm designing a power adapter as below:

- Power: 18W - 20W

- 1 USB-Type C port (Support QC4+)

- 1 USB-Type A port (Support QC 2, 3)

I'm using your chipset (TEA19051). But i don't understand how to design this product have two output (1 USB-Type C and 1 USB-Type A) that using one chipset (TEA19051).

Can you help me?

4 返答(返信)

2,293件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

You need two outputs with one TEA19051,right?

Sorry that can you tell us where you find some information about one TEA19051 support two channels outputs? I want to make sure I didn't miss something.

2,293件の閲覧回数
hoangdaive
Contributor II

Hi,

Thanks for your reply!

I see in the datasheet have some information as below:

Support:

- USB Type-C v.1.3

- USB Power Delivery (USB-PD) 2.0 and 3.0 including Programmable Power Supply
(PPS)

- Supports Qualcomm® QuickCharge™ QC2.0, QC3.0, and QC4+ protocols

- Battery Charging 1.2 (BC 1.2)

So, I want to designing a product that support two channels outputs!

0 件の賞賛
返信

2,293件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

Yes,it can support such topology but only can support one channel output.

2,293件の閲覧回数
hoangdaive
Contributor II

Hi,

Yes, thank you so much!

0 件の賞賛
返信