Questions about the PCA954X I2C bus switch

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Questions about the PCA954X I2C bus switch

629 次查看
Chromate
Contributor I
    I'm currently using the I2C switch PCA9545 and PCA9548 in my design, and I have several questions about the output pin.
    1) Are the SDn/SCn output pins open-drained? Judging from the necessity of pull-up resistors, we assume they are open-drained, but no evidence can be found in the datasheet.
    2) In the datasheet, the voltage translation is explained by an instance, in which the upstream bus has the highest voltage (5V) among all of the downstream buses (3.3V and 2.7V), and the design guide demands that the PCA954X should be powered with the lowest I2C bus voltage(2.7V) . My question is whether it is okay when upstream voltage is lower than (and furtherly, the lowest in) all of the downstream buses? For instance, if the SDA/SCL input is 1.8V, and all SDn/SCn is 3.3V, should we power the PCA954X switch with VDD=1.8V?
标记 (2)
0 项奖励
回复
3 回复数

584 次查看
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

Yes, they are open-drain, pull-up resistors are REQUIRED on all upstream and downstream channels.

Yes, you should power the PCA954X switch with VDD=1.8V. The multiplexers/switches should be supplied with the lowest I2 C voltage needed to ensure proper voltage translation.

Please find more information here: https://www.nxp.com/docs/en/application-note/AN262.pdf

Hope this helps.

0 项奖励
回复

579 次查看
Chromate
Contributor I
Thank you for your reply!

According to the PCA9545 datasheet, the operating power supply range is 2.3 V to 5.5 V, so is it okay to power it at Vdd=1.8V?
0 项奖励
回复

572 次查看
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

Yes, you are right, please use the VDD within the limits.

0 项奖励
回复