Question about TJA1021: SLP_N PIN pull-up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about TJA1021: SLP_N PIN pull-up

1,559 Views
YUANYUAN1
Contributor II

Hi all,

I met something not sure, here is the problems:

1. do I need to pull up SLP_N pin? I see the official development board pulls up it.

2. If I pull up SLP_N pin with the voltage powered on earlier than VBAT=12V, will it do harm to the chip?

Here is the circuit, VDD3V3 will power on ealier than VDD12V

YUANYUAN1_0-1667546508241.png

Best Regards,

Yuanyuan.

0 Kudos
Reply
1 Reply

1,546 Views
guoweisun
NXP TechSupport
NXP TechSupport

1: No problem.

2:Yes, you can.

3:No problem.

0 Kudos
Reply