Question about PTN3356

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about PTN3356

783 Views
lucarigazio
Contributor I


Hello,

I need to design a DisplayPort to VGA converter that works from -20° C to 85° C. PTN3356 would be perfect, but it does not work below 0° C. Are there any other solutions with NXP products? Which issues could I run into if I insist working with that device below 0° C ? Is there any way of getting samples tested/qualified in the industrial temperature range?

Thanks

0 Kudos
Reply
0 Replies