QSPI controller as SPI controller

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

QSPI controller as SPI controller

651 次查看
Nareshvarikuntla
Contributor III

Dear NXP,

I need additional SPI controller for my board based on LS1046. So I would like use existing QSPI controller as SPI controller.

Is it possible to configure QSPI controller as SPI controller. If yes, Please share relevant information on it.

Regards,

Naresh V. 

标记 (2)
0 项奖励
回复
1 回复

640 次查看
ufedor
NXP Employee
NXP Employee

qSPI can work with non-flash device as long as it meets the timing spec. You can have up to 16 LUT sequences to deal with different slaves, which is not necessary flash devices.

qSPI does not support Mode 1 operation as it drives data on falling edge and samples data on rising edge.

qSPI does not support slave mode.

Refer to the QorIQ LS1046A Reference Manual, 27.6.3.5 Issuing SFM Commands and the following presentation:

https://www.nxp.com/webapp/Download?colCode=FTF-NET-F0008&location=null

 

0 项奖励
回复