Hi, Im having troubles trying to load an SDK to MCUxpresso IDE, i download them from the SDK builder from NXP and i make them only for MCUxpresso IDE. But it continues to show me the error that the SDK is incorrect or that the SDK is NULL.
Already tried different SDKs for different boards, re-install MCUxpresso and nothing seems to work.
Could you tell me what can i do to fix this problem?
FYI im working with the 11.7.1_9221 version.
#MCUXpresso #IDE #Help
解決済! 解決策の投稿を見る。
Hello @VictorPastrana
The SDK2.14 doesn't support MCUXpresso IDE v11.7, need V11.8, while the IDE v11.8 have not released, so please download SDK2.13 to use.
Detail you can have a look at below thread:
BR
Alice
Thanks a lot, Alice!!
Hello @VictorPastrana
The SDK2.14 doesn't support MCUXpresso IDE v11.7, need V11.8, while the IDE v11.8 have not released, so please download SDK2.13 to use.
Detail you can have a look at below thread:
BR
Alice