Possibly a simple calc error? P82B715

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Possibly a simple calc error? P82B715

823 次查看
danielburgess
Contributor I

I have a question about something on the datasheet for P82B715, link provided below.

http://www.nxp.com/documents/data_sheet/P82B715.pdf

On page 7 it says:

"In this example that is 1 kΩ || 10 kΩ || 10 kΩ = 833 Ω. For a 5.5 V supply and 0.4 V LOW, that means the buffer is sinking 16.3 mA."

I cannot see how 16.3mA was calculated. Using V=IR, to calculate current, I=V/R, 5V/833Ω = 6.1mA <- that's what I get.

Can someone help out here? Is this a typo or is my math off?

Please and thanks.

标记 (2)
0 项奖励
回复
0 回复数