Porting Guide for NXP-NCI example

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Porting Guide for NXP-NCI example

1,312 次查看
Shikamaru
Contributor I

I donwloaded the NXP-NCI_example v1.3 for windows from the below link https://www.mikroe.com/nfc-usb-dongle. I tried out the given samples and played little here and there. However I have some requirement of porting this example to stm32 controller or STM MCU we can say. (My stm32 board will be Host for that am attaching this dongle to communicate) How can I proceed, what will be the challenges .Kindly guide me here.

Regards,

Shikamaru

0 项奖励
回复
1 回复

1,289 次查看
KaiLi
NXP TechSupport
NXP TechSupport

Hello @Shikamaru 

The USB dongle is a product designed based on NXP's NFC and MCU. This is a third-party product and is not a product of NXP. This USB dongle implements all the features of the PN7150 reader, and its external interfaces include NFC and USB. Based on your design requirements, I understand that it should be integrated into your STM32 system through the USB interface. If this is the case, what you need to do is what is the communication protocol of the USB dongle to external communication through the USB interface, and then your STM32 end can also implement the same protocol, because the NFC behavior and performance is completed by the USB dongle. Unfortunately, USB dongle is not a terminal product of NXP, we are not such a protocol, so it is recommended that you consult MIKROE. Hope to make myself clear.

BR

kelly

0 项奖励
回复