Packet Forwarding Engine for S32G

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Packet Forwarding Engine for S32G

3,599 次查看
muhammad_qasim
Contributor I

Hi

Is Packet Forwarding Engine is mandatory for Gigabit Ethernet Media Access Controller (GMAC; Synopsys DesignWare Universal Ethernet MAC) on S32G? This GMAC IP is shared on multiple platforms like cyclone_v_soc where PFE is not being used.

If yes, where we can get the register set for Packet forward engine for S32G?

What is the version of Synopsys MAC controller?

Regards 

 

0 项奖励
回复
4 回复数

3,561 次查看
muhammad_qasim
Contributor I

Thanks for your help. 

Can we get Packet Forward Engine documentation on DocStore?

0 项奖励
回复

3,554 次查看
bpe
NXP Employee
NXP Employee

Documentation with restricted access and the ways to obtain it cannot be discussed on a public forum. If you need assistance with it, please open a Support Case

 

Best Regards,
Platon

0 项奖励
回复

3,551 次查看
muhammad_qasim
Contributor I

Great. Thanks 

0 项奖励
回复

3,575 次查看
bpe
NXP Employee
NXP Employee

GMACs on S32G processors are owned by PPFE. Only a very small part of GMAC functionality
is controlled directly by software. The rest is abstracted by PPFE which is a microcode-
controlled machine. PPFE programming interface details are currently available only to
authorized customers. If you are planning a design with S32G, please contact your distributor
for assistance.

Best Regards,
Platon

 

 

0 项奖励
回复