Hello @Rakesh_Kumar-Thakur
I hope you are doing very well.
Please take a look to the imx93-11x11-evk-boe-wxga-lvds-panel.dts on the kernel git.
There you can see the node called lvds_backlight: lvds_backlight:
lvds_backlight: lvds_backlight {
compatible = "pwm-backlight";
pwms = <&adp5585pwm 0 100000 0>;
enable-gpios = <&adp5585gpio 8 GPIO_ACTIVE_HIGH>;
power-supply = <®_vdd_12v>;
status = "okay";
brightness-levels = < 0 1 2 3 4 5 6 7 8 9
10 11 12 13 14 15 16 17 18 19
20 21 22 23 24 25 26 27 28 29
30 31 32 33 34 35 36 37 38 39
40 41 42 43 44 45 46 47 48 49
50 51 52 53 54 55 56 57 58 59
60 61 62 63 64 65 66 67 68 69
70 71 72 73 74 75 76 77 78 79
80 81 82 83 84 85 86 87 88 89
90 91 92 93 94 95 96 97 98 99
100>;
default-brightness-level = <80>;
};
You can see the pwms property is calling to the node adp5585pwm defined on imx93-11x11-evk.dts. Pin 3 (R3 of the adp5585).
The default brightness level is 80 and you can change it on user space:
root@imx93evk:/sys/class/backlight/lvds_backlight# echo 90 > brightness
Alejandro_Salas_0-1731695583736.png
root@imx93evk:/sys/class/backlight/lvds_backlight# echo 100 > brightness
Alejandro_Salas_1-1731695629280.png
root@imx93evk:/sys/class/backlight/lvds_backlight# echo 50 > brightness
Alejandro_Salas_2-1731695667674.png
I hope this information can helps to you!
Best regards,
Salas.