PTN3392BS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PTN3392BS

1,751 次查看
aizikz
Contributor I

Dear Team

we have received PTN3392BS from NXP

is there any way of knowing which firmware version is burnt on the device without connecting it ?

maybe there is something on the label we can use to identify the firmware?

Aizik

0 项奖励
回复
3 回复数

1,684 次查看
aizikz
Contributor I

hi Jose,

thank you for the reply , unfortunately the PN listed ob the label is only PTN3392BS,518

i attached the picture below!

pastedImage_1.jpg

0 项奖励
回复

1,684 次查看
reyes
NXP TechSupport
NXP TechSupport

Hi,

 

Then you can identify them using the NXP’s 12NC number (MPN), which for the PTN3392BS,518 is 935288181518 as you can see in the product details page: https://www.nxp.com/part/PTN3392BS

 

PTN3392BS (without the “/Fx” suffix in the part number) is the PTN3392 with latest production firmware (Trust NXP). The production version 4.0 is programmed in PTN3392BS (Trust NXP).

There is no other way to knowing which firmware version is burnt on the device without connecting it.

 

Regards,

Jose

NXP Semiconductors

0 项奖励
回复

1,684 次查看
reyes
NXP TechSupport
NXP TechSupport

Hi Aizik,

 

PTN3392BS should be shipped with a label on the packing with the part number like PTN3392BS/Fx, where the ‘x’ represent the firmware version as follows:

* PTN3392BS/F4: PTN3392 with production firmware version 4.0.

* PTN3392BS/F3: PTN3392 with production firmware version 3.0.

* PTN3392BS/F2: PTN3392 with production firmware version 2.0.

* PTN3392BS/F1: PTN3392 with production firmware version 1.0.

* PTN3392BS: PTN3392 with latest production firmware (Trust NXP). The production version 4.0 is programmed in PTN3392BS (Trust NXP).

0 项奖励
回复