PTN3222 as USB2 to eUSB2 host

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PTN3222 as USB2 to eUSB2 host

1,728 Views
alex0800
Contributor I

Is it possible to configure PTN3222 as Host-USB2 to eUSB2 host?

I other words, can PTN3222 convert a normal USB2 host port to eUSB2 host?

0 Kudos
Reply
5 Replies

1,708 Views
alex0800
Contributor I

More specifically, I am interested if the following configuration would allow me to exercise all normal USB2 traffic:

CFG2.png

 

0 Kudos
Reply

1,697 Views
RafaR
NXP Employee
NXP Employee

Hi Alex

Sorry, unfortunately your design will not work.

PTN3222 eUSB side has to be connected to a controller, either Host or Devise.

 

Have a great day and best of luck.

0 Kudos
Reply

1,283 Views
jia1
Contributor I

Hi Rafer,

I configured register 0x02 of repeater 1 to 0x22 (Force Device role & Force the repeater into its
Connect) and register 0x02 of repeater 2 to 0x12 (Force Host role & Force the repeater into its
Connect) through the I²C interface. I captured the waveform with a logic analyzer and found that the SOF packet sent by the host on the USB side of repeater 1 can be received normally on the USB side of repeater 2. Does this mean that this connection mode is feasible?

0 Kudos
Reply

1,708 Views
alex0800
Contributor I

Hello Rafar,

No, I mean the following configuration:

CFG1.png

 

0 Kudos
Reply

1,712 Views
RafaR
NXP Employee
NXP Employee

Hi Alex

I'm not sure if I understand you correctly

Do you mean this?

RafaR_0-1740594507437.png

 

0 Kudos
Reply