PSMN1R0-30YLD MOSFET Spice Models

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PSMN1R0-30YLD MOSFET Spice Models

1,570 Views
lev_nemets
Contributor I

Hello,

I found that Spice model for PSMN1R0-30YLD MOSFET perfectly coincides with datasheet. This is great. Is it possible to change some model parameters in order to simulate worst case conditions: Maximum Rdson, Qg(tot), minimum and maximum Vgs(th)?

Thanks

Lev

0 Kudos
Reply
1 Reply

1,509 Views
nxf45548
NXP Employee
NXP Employee

PSMN1R0-30YLD was transferred to Nexperia on 06-Feb-2017. 
Please contact directly with them for further assistance

PSMN1R0-30YLD - N-channel 30 V, 1.0 mΩ, 300 A logic level MOSFET in LFPAK56 using NextPowerS3 Techno... 

0 Kudos
Reply