PSMN1R0-30YLD MOSFET Spice Models

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PSMN1R0-30YLD MOSFET Spice Models

1,548 次查看
lev_nemets
Contributor I

Hello,

I found that Spice model for PSMN1R0-30YLD MOSFET perfectly coincides with datasheet. This is great. Is it possible to change some model parameters in order to simulate worst case conditions: Maximum Rdson, Qg(tot), minimum and maximum Vgs(th)?

Thanks

Lev

0 项奖励
回复
1 回复

1,487 次查看
nxf45548
NXP Employee
NXP Employee

PSMN1R0-30YLD was transferred to Nexperia on 06-Feb-2017. 
Please contact directly with them for further assistance

PSMN1R0-30YLD - N-channel 30 V, 1.0 mΩ, 300 A logic level MOSFET in LFPAK56 using NextPowerS3 Techno... 

0 项奖励
回复