PN7150 High Bitrate

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,757件の閲覧回数
wilmer_suarez
Contributor III

Hello,

I'm using a PN7150 to communicate with an NFC endpoint that supports the ISO-DEP protocol. I was reading the user manual and it states that "... the ISO-DEP RF interface activation for technology NFC-A is incompatible with bit rates higher than 106kbps...". But it also states that higher bit rates can be used for NFC-A technologies.

Is there a workaround that will allow me to configure the transmission of the PPS command by the Host or by the PN7150, to allow the higher bit-rates?

 

Thanks 

タグ(2)
0 件の賞賛
返信
1 解決策
4,745件の閲覧回数
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hi @wilmer_suarez ,

Hope you are doing great, as you correctly state, the reader supports 106, 212,424 and 848 speeds, in the user manual you can also find in section 6.3.6 the explanation of this and a  part of the NCI specs,  how the PI_BIT_RATE  can be used to do this.

jonathaniglesia_0-1603726485788.png

 

BR

 

Jonathan

元の投稿で解決策を見る

5 返答(返信)
4,746件の閲覧回数
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hi @wilmer_suarez ,

Hope you are doing great, as you correctly state, the reader supports 106, 212,424 and 848 speeds, in the user manual you can also find in section 6.3.6 the explanation of this and a  part of the NCI specs,  how the PI_BIT_RATE  can be used to do this.

jonathaniglesia_0-1603726485788.png

 

BR

 

Jonathan

4,741件の閲覧回数
wilmer_suarez
Contributor III

Hi @Jonathan_Iglesias,

Section 6.3.6 also states:

"Everything is prepared (see the RF configuration parameter PI_BIT_RATE), except for the ISO-DEP RF Interface activation. As currently defined in [NCI], the ISO-DEP RF interface activation for technology NFC-A is incompatible with bit rates higher than 106kbps, since this requires to handle the PPS commands exchange, which is not addressed in [NCI]."

If I set the PI_BIT_RATE to 848 kbps, would it maintain when communicating through the ISO-DEP RF interface?

If no, is there another way to handle the PPS exchange, either through the DH or the NFCC?

 

Thanks

0 件の賞賛
返信
4,729件の閲覧回数
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

yes you are correct, so in the same chapter there are some modifications  that are the ones I sent in my first reply:

jonathaniglesia_0-1603747518242.png

so there is a little modifications (first reply) from the ISO-DEP. 

Have a great day !  

Jonathan 

 

4,714件の閲覧回数
wilmer_suarez
Contributor III

Ah, sorry. I misunderstood the wording in the manual. So, by "an allowed value higher than 0x00" means any of the 4 standard rates? 

0 件の賞賛
返信
4,702件の閲覧回数
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

yes that is correct, other value of bit rate.

BR

 

Jonathan

0 件の賞賛
返信