PN5180 issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PN5180 issue

3,336 次查看
chris_zhang
Contributor II

Hi,

We have a new projects that need to use NFC readers, and initially plan to use PN5180, the reading standard is ISO14443;

Now we needs to modify the differential output of the antenna part to a single-ended output, and use the RF switch to split the single-ended output signal into two channels, that is, according to the figure below, after matching the antenna to 50ohm, then divide the TX into TX1/TX2/ TX3/TX4, access to different antennas;
标签 (1)
  • RF

标记 (2)
2 回复数

3,276 次查看
IvanRuiz
NXP Employee
NXP Employee

Hello,

Please accept my apologies but this has not been tested by us since all of our designs use both, TX1 and TX2 outputs and one antenna. Nevertheless, with a single-ended design only please consider that the output power will be reduced by 3dB (half).

Hope it helps!

BR,

Ivan.

0 项奖励
回复

3,276 次查看
chris_zhang
Contributor II

Hi Ivan,

Fine, we will double chekc the available of this solution, thanks for your comment.