PF0100 PMIC Automated Programming via KITPFPGMEVME

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PF0100 PMIC Automated Programming via KITPFPGMEVME

2,021 Views
petervuong
Contributor I

Hello,

I'm currently trying to program a MMPF0100F9AZES with a KITPFPGMEVME (REV B) PF Series Programmer.  I am able to program via the recommended KITPFGUI application successfully.  I was hoping to automate the process via a command line interface as opposed to the GUI.  Suggestions or recommendations?

Thanks for any assistance anyone may provide!
Peter

0 Kudos
Reply
3 Replies

1,873 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Peter,

It is very unfortunate for me to let you know that we do not have any recommendation about how to automate the process of OTP programming via command line interface.

I apologize for the problem this may cause.

 

However, there is an option in the KITPFGUI that can be enabled using the KIPFPGMEVME that allows the user to program multiple devices, in the Programming tab, there is a check box named “Program multiple Parts”.

I hope this can be helpful.


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,873 Views
petervuong
Contributor I

Hello Jose,

Thanks for getting back to me on this issue.  Can you please clarify what you had said in a previous related post when you mentioned "Some of our customers have developed their own ‘command line’ interface that works with the PF-programmer board"?  What exactly is the "PF-programmer board"?  Were you referring to the KITPF0100SKTEVBE?

Thanks!

Peter

0 Kudos
Reply

1,873 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Peter,

When I mentioned “PF-Programmer board” I was referring to the KITPFPGMEVME (REV B) PF Series Programmer.

pastedImage_1.png

The PF-Programmer works only with either the Socket Board (KITPF0100SKTEVBE) or your own target hardware provide that have included the 8-pin header we suggest in our Users Guide.

Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply