PCF8576C

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PCF8576C

2,277 次查看
kebronmichael_w
Contributor I

I'm working with a single PCF8576C and I'm not sure where to connect the CLK and SYNC pin in static mode. 

The datasheet says that those pins should be at a defined level(Vss or Vdd). 

I'm using the internal oscillator of the PCF8576C that means I get an output clock signal from CLK for cascaded PCF8576. Can I simply pull both pins up ? 

Thanks in advance!

标记 (2)
3 回复数

2,196 次查看
guoweisun
NXP TechSupport
NXP TechSupport

HI

If you use single PCF8576C no the cascaded application,pins SYNC and CLK must be left open circuit.

Thanks!

2,196 次查看
kebronmichael_w
Contributor I

Thank you! 

Is it mandatory to leave them open circuit or can I also pull/push them to Vdd/Vss ? 

0 项奖励
回复

2,196 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Hi

It's mandatory to leave them open circuit

0 项奖励
回复