PCF8576C

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCF8576C

2,250件の閲覧回数
kebronmichael_w
Contributor I

I'm working with a single PCF8576C and I'm not sure where to connect the CLK and SYNC pin in static mode. 

The datasheet says that those pins should be at a defined level(Vss or Vdd). 

I'm using the internal oscillator of the PCF8576C that means I get an output clock signal from CLK for cascaded PCF8576. Can I simply pull both pins up ? 

Thanks in advance!

タグ(2)
3 返答(返信)

2,169件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

HI

If you use single PCF8576C no the cascaded application,pins SYNC and CLK must be left open circuit.

Thanks!

2,169件の閲覧回数
kebronmichael_w
Contributor I

Thank you! 

Is it mandatory to leave them open circuit or can I also pull/push them to Vdd/Vss ? 

0 件の賞賛
返信

2,169件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi

It's mandatory to leave them open circuit

0 件の賞賛
返信