PCF8566

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCF8566

713 Views
ben_redmon
Contributor I

I am looking for a specification for the expected frequency min/max of the built-in internal oscillator (fosc) of the PCF8566 LCD Driver IC. The spec sheet only lists a range for fclk, which can be externally supplied or set to be fosc, as ranging from 125kHz to 315kHz. Does this mean that the internal oscillator (fosc) can have such a wide range of possible frequencies?

Tags (1)
0 Kudos
Reply
1 Reply

667 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi

Yes,the internal oscillator (fosc) can have such a wide range of possible frequencies!

0 Kudos
Reply