PCF85363A Power-up question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCF85363A Power-up question

1,034 Views
michaelolson
Contributor I

I am using a PCF85363A with a back-up battery. If the chip is powered up with the back-up battery first, the INTA output puts out 32.768kHz when VDD is applied. If it is powered with VDD first, the INTA output is at 1 sec. Is that correct operation?

0 Kudos
Reply
1 Reply

926 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Michael,

Sorry for our late response.  

At VDD power up, all PCF85363A registers should be reset in Default Mode. As stated on page 55 of the data sheet, the default frequency on INTA/ pin should be 32.768 kHz.
image006.png
image007.png
Best regards,
Tomas
0 Kudos
Reply