I am looking into using the PCF85263ATL/AX real time clock component. During evaluation of the data sheet, I noticed that Pin-4(TS/CLK/INTB_n) is not connected if the input is not used; however, I cannot seem to find what to do with pin-9, INTA_n/CLK, and pin-8, CLK. I don't just want to leave these unconnected so am looking for what is recommended for these pins if they are not being used.
Hello Robert,
You can leave the Pin 9 INTA_n/CLK and Pin 8 CLC unconnected if they are not being used. You can also check the user manual UM10301 for NXP Real Time Clocks here (section 16).
Have a great day,
Paulina