PCA9685

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCA9685

2,180 Views
bilibilimisaka1
Contributor I

IMG_20180923_230026.jpg

I use the Raspberry Pi3+ and pca9685 to control 20 standard servos. The power supply is 6v. However, when driving them, the height calculation error causes the servo to not move. As a result, the board burns here. I want to ask if it can be used?#pca9685

Tags (1)
0 Kudos
Reply
1 Reply

2,096 Views
lisettelozano
NXP Employee
NXP Employee

Hello X YY,

 

You may want to use separate power supplies to meet with the limiting values for the PCA9685. Please note table 13 and table 14 from datasheet where states the operating power supply voltage (VDD) range of 2.3V to 5.5V and supply current (IDD) is 6mA to 10mA; with a 5.5V tolerant inputs (VI/O).

 

I hope this information can be helpful.

 

Have a great day,

Paulina

0 Kudos
Reply