PCA9685 drive frequency tolerance details

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PCA9685 drive frequency tolerance details

864 次查看
__invited__hari
Contributor V

Hello NXP,

 

We are heavily using PCA9685 in our products. I see that it uses an internal clock of 25MHz to drive LEDs, but no tolerance details available. I configured those channels to output 900kHz but the measured value is about 850kHz and this value varies between ICs. Can you please help us with the tolerance details and also the temperature variation details? This is very important for our characterization study. Please support with those details at the earliest.

 

Thanks,

Hari

0 项奖励
回复
5 回复数

842 次查看
__invited__hari
Contributor V

Thanks, Tomas, for the quick turnaround.

Can you please share those details about what leads to that 20% variation? Some temperature graphs or any other drift details, etc...

0 项奖励
回复

793 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Hari,

The PCA9685 is approximately 15 years old and unfortunately all designers are gone. I do not have access to the information such as temperature graphs or other drift details, sorry about that.

BR, Tomas

0 项奖励
回复

785 次查看
__invited__hari
Contributor V

Understood. Thank you for the clarification.

0 项奖励
回复

804 次查看
__invited__hari
Contributor V

Hello NXP,

 

Can someone please respond with the requested details soon?

 

Thanks,

Hari

0 项奖励
回复

850 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Hari,

The internal 25MHz oscillator in the PCA9685 is untrimmed and has something like a +/-20% variation.

BR, Tomas

0 项奖励
回复