PCA9685 drive frequency tolerance details

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCA9685 drive frequency tolerance details

1,344 Views
__invited__hari
Contributor V

Hello NXP,

 

We are heavily using PCA9685 in our products. I see that it uses an internal clock of 25MHz to drive LEDs, but no tolerance details available. I configured those channels to output 900kHz but the measured value is about 850kHz and this value varies between ICs. Can you please help us with the tolerance details and also the temperature variation details? This is very important for our characterization study. Please support with those details at the earliest.

 

Thanks,

Hari

0 Kudos
Reply
5 Replies

1,322 Views
__invited__hari
Contributor V

Thanks, Tomas, for the quick turnaround.

Can you please share those details about what leads to that 20% variation? Some temperature graphs or any other drift details, etc...

0 Kudos
Reply

1,273 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Hari,

The PCA9685 is approximately 15 years old and unfortunately all designers are gone. I do not have access to the information such as temperature graphs or other drift details, sorry about that.

BR, Tomas

0 Kudos
Reply

1,265 Views
__invited__hari
Contributor V

Understood. Thank you for the clarification.

0 Kudos
Reply

1,284 Views
__invited__hari
Contributor V

Hello NXP,

 

Can someone please respond with the requested details soon?

 

Thanks,

Hari

0 Kudos
Reply

1,330 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Hari,

The internal 25MHz oscillator in the PCA9685 is untrimmed and has something like a +/-20% variation.

BR, Tomas

0 Kudos
Reply