PCA9685 Restart Counter...

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCA9685 Restart Counter...

ソリューションへジャンプ
2,181件の閲覧回数
Sehnsucht
Contributor I

Is there a way to reset the counter without having to sleep/wake or reset the chip?

 

Here is the application: Using the PCA9685 to control PWM outputs to trailing edge AC dimmers such that the leading edge of all the PWM rising edges should happen at the AC zero cross point. So We need a way to force all the channels to have a rising edge with a trigger signal. The OE pin does not work for this since it just turns the signal on and off at the same point it would otherwise. Sleep/wake works but there is a 500us delay which is an eternity in PWM world.

 

It would be fantastic if we had a way to reset the internal counter to 0 with a pin or I2C command which would solve this problem. 

 

Appreciate your time in advance.

 

0 件の賞賛
返信
1 解決策
2,167件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Masoud,

I am afraid there is no way to reset the counter using an I2C command or a pin, unfortunately.

Regards,

Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,168件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Masoud,

I am afraid there is no way to reset the counter using an I2C command or a pin, unfortunately.

Regards,

Tomas

0 件の賞賛
返信