PCA9685 LED driving

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCA9685 LED driving

4,077 Views
JohnJohnny
Contributor I

Hello,

I would like to use the PCA9685 to drive bicolor LEDs (2-pin LEDs, color changes when the current in the LED is reversed).

I am thinking of connecting my LEDs between 2 pins of a PCA9685, let's say OUT1 and OUT2.

If OUT1 is set to HIGH, I can control the brightness of color 1 by applying PWM to OUT2.

If OUT2 is set to HIGH, I can control the brightness of color 2 by applying PWM to OUT1.

If OUT1 and OUT2 are LOW,  LED is off.

Could you confirm me this is possible?

0 Kudos
Reply
5 Replies

4,019 Views
JohnJohnny
Contributor I

Hello,

my question in a more general way would be:

can I drive 2-pin bi-color LEDs with the PCA9685, in a way that allow me to use both colors of the same LED (not at the same time) and control their brightness?

I'm thinking of configuring all the outputs in totem pole. Let's say LED1 is between OUT1 and OUT2 with a series resistor.
OUT1 PWM duty cycle = 100% and OUT2 PWM cycle = 0%, LED is red, full brightness
OUT1 PWM duty cycle = 50% and OUT2 PWM cycle = 0%, LED is red, medium brightness
OUT1 PWM duty cycle = 0% and OUT2 PWM cycle = 100%, LED is green, full brightness
OUT1 PWM duty cycle = 0% and OUT2 PWM cycle = 50%, LED is green, medium brightness

Does this work?

0 Kudos
Reply

4,000 Views
guoweisun
NXP TechSupport
NXP TechSupport

I am afraid that it doesn't work!

 

0 Kudos
Reply

4,039 Views
guoweisun
NXP TechSupport
NXP TechSupport

HI

Could you please send us the application block diagram for better comprehend ?

 

0 Kudos
Reply

4,034 Views
JohnJohnny
Contributor I

Hey,

here is an example of what I intend to do. It features 3 push buttons that have internal bi-color LEDs. I've seen that PCA9685 outputs can source and sink current, this is why I imagine this is possible.

In the final application they would be 24 bi-color LEDs driven by 3 PCA9685.

0 Kudos
Reply

4,026 Views
guoweisun
NXP TechSupport
NXP TechSupport

Thanks for your feedback!
But I still can't fully understand!

Could you please give one channel complete circuit for example sent OUT1 high and generate PWM on OUT2?

 

0 Kudos
Reply