Both devices support I2C communication with Fast-mode Plus (1 MHz) and share the same register structures with default settings. The slave address is also identical. So, I believe that no FW changes are necessary.
I am using the PCA9632DP2Z to drive a 12V RGB LED. Since this IC operates at 5V, I have incorporated a transistor driver circuit. Kindly review the circuit below and share your feedback or suggestions
Both devices support I2C communication with Fast-mode Plus (1 MHz) and share the same register structures with default settings. The slave address is also identical. So, I believe that no FW changes are necessary.