Dear Experts,
We want to use "PCA9616" in our IO-system project. There will be 25 devices connected on the dI2C bus working on FM+ 1 MHZ. Maximum Cb = 400 pf. The maximum bus length is less than 50 cm but in a harsh environment, so we decided to use the dI2C.
Our question is about the propagation delay on FM+ 1 MHZ. From the datasheet:
Max. Tphl (single-ended side to differential side) = 120 ns.
Max. Tphl (differential side to single-ended side) = 150 ns.
Which leads to, total maximum propagation delay of master to slave path = 270 ns.
The return path from slave to master (for example to send ack. or data) = 270 ns.
Accordingly, the total maximum propagation delay of the round-trip path = 540 ns.
I understand that slave must put the reply (ack. or data) on the falling edge of the clock and the master must read this data on the rising edge of the clock. This period <= 500 ns on 1 MHZ.
So, if I correctly understand then the device "PCA9616" will not work on FM+ 1 MHZ.
Please explain to us what correct propagation delay on FM+ 1 MHZ is? And how we can use "PCA9616" on this speed.
Regards,
Medhat.