PCA9614 overheating

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCA9614 overheating

2,970件の閲覧回数
gb88
Contributor I

Hi, i made a circuit with the PCA9614, the circuit is working great but the temperature of the PCA9614 is around 150 °C, i don't even know how is possible that is still working, the circuit seem correct, what could be the cause of this overheating?

Thanks

0 件の賞賛
返信
4 返答(返信)

2,652件の閲覧回数
sd23
Contributor I

Is the problem solved?

0 件の賞賛
返信

2,818件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

Please pay attention on the maximum power dissipation is 100mW on application.

Please make sure whether out of range of PCA9614.

Thanks!

0 件の賞賛
返信

2,818件の閲覧回数
gb88
Contributor I

Hi, i know that the temperature is out of range, but the point is that everything seems in range. Here the circuit, the PCA9614 is overheating also with the differential bus open. The Vdd is 3.3V regulated.bus.jpg

0 件の賞賛
返信

2,818件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

Please also test the IDD when differential bus open to check the power consumption.

0 件の賞賛
返信