PCA9614 overheating

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCA9614 overheating

2,969 Views
gb88
Contributor I

Hi, i made a circuit with the PCA9614, the circuit is working great but the temperature of the PCA9614 is around 150 °C, i don't even know how is possible that is still working, the circuit seem correct, what could be the cause of this overheating?

Thanks

0 Kudos
Reply
4 Replies

2,651 Views
sd23
Contributor I

Is the problem solved?

0 Kudos
Reply

2,817 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

Please pay attention on the maximum power dissipation is 100mW on application.

Please make sure whether out of range of PCA9614.

Thanks!

0 Kudos
Reply

2,817 Views
gb88
Contributor I

Hi, i know that the temperature is out of range, but the point is that everything seems in range. Here the circuit, the PCA9614 is overheating also with the differential bus open. The Vdd is 3.3V regulated.bus.jpg

0 Kudos
Reply

2,817 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

Please also test the IDD when differential bus open to check the power consumption.

0 Kudos
Reply