PCA9614 overheating

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PCA9614 overheating

3,027 次查看
gb88
Contributor I

Hi, i made a circuit with the PCA9614, the circuit is working great but the temperature of the PCA9614 is around 150 °C, i don't even know how is possible that is still working, the circuit seem correct, what could be the cause of this overheating?

Thanks

0 项奖励
回复
4 回复数

2,709 次查看
sd23
Contributor I

Is the problem solved?

0 项奖励
回复

2,875 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

Please pay attention on the maximum power dissipation is 100mW on application.

Please make sure whether out of range of PCA9614.

Thanks!

0 项奖励
回复

2,875 次查看
gb88
Contributor I

Hi, i know that the temperature is out of range, but the point is that everything seems in range. Here the circuit, the PCA9614 is overheating also with the differential bus open. The Vdd is 3.3V regulated.bus.jpg

0 项奖励
回复

2,875 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

Please also test the IDD when differential bus open to check the power consumption.

0 项奖励
回复