PCA9535A GPIO expander

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCA9535A GPIO expander

2,246 Views
arios100
Contributor I

Hello, 

I have the reset signal going to the PCA9535A reset input being driven by a 3.3V signal but the PCA9535A is being powered by 1.8V VDD. Is this allowed? The datasheet says its 5V tolerant. 

arios100_0-1647924952059.pngarios100_0-1647924952059.png

 

0 Kudos
Reply
4 Replies

2,242 Views
arios100
Contributor I

the PCA9539A is from 1.65 to 5.5V see below.

arios100_0-1647925879824.pngarios100_0-1647925879824.png

 

0 Kudos
Reply

2,239 Views
guoweisun
NXP TechSupport
NXP TechSupport

Understand, please connect the RESET pin to VDD.

 

0 Kudos
Reply

2,236 Views
arios100
Contributor I

I don't have a 1.8V  output reset signal, only have the 3.3V reset signal. 

Are you saying that reset input is not 3.3V tolerant when gpio's VDD is 1.8V?

0 Kudos
Reply

2,244 Views
guoweisun
NXP TechSupport
NXP TechSupport

Please get note that the VDD range is from 2.3V to 5.5V, the 1.8V can't be used.

 

 

0 Kudos
Reply