P1014 QorIQ Integrated Processors

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P1014 QorIQ Integrated Processors

1,029 Views
PTusername
Contributor I

In case of P1014 QorIQ Integrated Processors

Link-  https://rocelec.widen.net/view/pdf/vr2ddso1wa/FSCLS11835-1.pdf?t.download=true&u=5oefqw

Please refer to Page 98, Table 86 last column in above link. .Are the die revs backward compatible?  Your help is highly appreciated.

E.g. Is P1014NXN5HHB  backward compatible to  P1014NXN5HHA?

 

 

 

 

0 Kudos
Reply
1 Reply

1,012 Views
yipingwang
NXP TechSupport
NXP TechSupport

The errata document for the p1010 which covers the p1014 as well. If you have this document, you can go through table 3 to identify which errata applies for Rev 1.0 "A" and Rev 2.01 "B" silicon of the P1014. Depending on the your use case and features that are enabled on the P1014, it may or may not be backward compatible.

0 Kudos
Reply