OM13069 Firmware

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OM13069 Firmware

2,402 Views
decchito
Contributor I

I'm planning buy OM13069 board.

So I'm looking for the firmware of it,

but I couldn’t find it.

Where is the firmware souce code of OM13069 board on NXP web site??

 I could find below 2 source code 

NXP® Quick Jack LPC800 LPCXpresso 1

NXP® Quick Jack LPC800 Keil IAR 0

But according to schematic of OM13069 board, LPC812 is mounted.

So, what these source code for?

Somebody ,please teach me...

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

2,239 Views
jeremyzhou
NXP Employee
NXP Employee

Hi yoshimasa yazawa,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
These above source codes are same except for base on different IDE.
Hope this helps.
Have a great day,

TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,239 Views
decchito
Contributor I

Hi,Jeremzhou.

thank you for yor reply.

I could understand.OK.

I thought that LPC800 is device name.

but it was my misunderstanding.

LPC800 is family name of LPC series.right?

So I thought that these 2 source code is not for OM13069 board.

Because, on OM13069 board, LPC812 is mounted.

Anyway, for OM13069 board,I can use both of these source code( depend on IDE ), right? 

0 Kudos
Reply

2,239 Views
jeremyzhou
NXP Employee
NXP Employee

Hi yoshimasa yazawa,

Thanks for your reply.

Anyway, for OM13069 board,I can use both of these source code( depend on IDE ), right? 

-- Yes, you're right
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply