Need Help with RF Power FET MRF6V2150NR1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Need Help with RF Power FET MRF6V2150NR1

1,666 次查看
s180010
Contributor II

Hello Everyone,

i am searching for a development/testing board fpr the MRF6V2150NR1 RF Power FET. I want verify the data from the NXP datascheet with our local enviiroment and set up a little thesis on that.

If somethign like that is not available do you maybe have a Eagle schematic layoutfile or something to rebuild the in and output nework on FR4 material?

I appriciate any answer and help.

Best regards,

Horst (German soon to be Master Engineer working for University) 

G
M
T
Die Sound-Funktion ist auf 200 Zeichen begrenzt
0 项奖励
回复
2 回复数

1,511 次查看
LPP
NXP Employee
NXP Employee

NXP offers several designs for MRF6V2150N. You can order these designs through our authorized distributors (RichardsonRFPD, Avnet, RFMW...). They can be ordered as a fully assembled and tested circuit or as a kit that includes PCB, device samples and all the components required.

Please, I sent you DXF file for 220MHz test circuit as it is described in the datasheet.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,511 次查看
s180010
Contributor II

Dear Pavel,

thank you for your answer! I did not receive an DXF file...

Anyway can you give me the link of an fully assambled Test circiut or an also one fpr the Kit with PCB?

I can not find it even if i type the you distributors.

Have a nice day,

Horst

0 项奖励
回复