NXP true anticollision

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP true anticollision

Jump to solution
2,318 Views
premtos
Contributor I

I have a question about NFC SLIX2, What is the difference between "NXP true anticollision" and "anticollision" in standard ISO/IEC15693 ?

Labels (1)
  • RF

0 Kudos
Reply
1 Solution
2,265 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @premtos ,

 

True anticollision means fully compatible with "anticollision" in standard ISO/IEC15693.

 

Hope that makes sense,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

2 Replies
2,249 Views
premtos
Contributor I

Thank you

0 Kudos
Reply
2,266 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @premtos ,

 

True anticollision means fully compatible with "anticollision" in standard ISO/IEC15693.

 

Hope that makes sense,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------