NXP true anticollision

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP true anticollision

ソリューションへジャンプ
2,338件の閲覧回数
premtos
Contributor I

I have a question about NFC SLIX2, What is the difference between "NXP true anticollision" and "anticollision" in standard ISO/IEC15693 ?

ラベル(1)
  • RF

0 件の賞賛
返信
1 解決策
2,285件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @premtos ,

 

True anticollision means fully compatible with "anticollision" in standard ISO/IEC15693.

 

Hope that makes sense,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,269件の閲覧回数
premtos
Contributor I

Thank you

0 件の賞賛
返信
2,286件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @premtos ,

 

True anticollision means fully compatible with "anticollision" in standard ISO/IEC15693.

 

Hope that makes sense,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------