NXP RTC PCF8563 Technical issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP RTC PCF8563 Technical issue

2,384件の閲覧回数
chenhuang
Contributor II

When commissioning PCF8563T, the customer found that VL bit of VL_seconds register of some chips was read as 0 when it was powered on for the first time. Theoretically, it should be 1.

The hardware side of the customer has done the timing test, and confirmed that there is no problem with the IIC timing. The hardware iic is used for communication. Not all chips are like this, and some chips have this phenomenon. Please help

Take a look at how to locate the problem and solve the customer's problem, and give some suggestions or doubts, thank you!

0 件の賞賛
返信
2 返答(返信)

2,377件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

尝试让客户power on以后等600ms再去通信。

 

0 件の賞賛
返信

2,376件の閲覧回数
chenhuang
Contributor II

好的,我这边让客户去尝试验证下,谢谢

0 件の賞賛
返信