NXP J3R180 hangs up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP J3R180 hangs up

3,591 Views
AlbertEin
Contributor I

Recently, I've purchased 5 test J3R180 cards for my project. Unfortunately, they hang when running long lasting commands in response to sending APDUs!

I asked about this from vendor (Alibaba), and they said "you have to initialize the card first" but "we cannot share any script with you"!

Can you help me to make these cards working so that I can continue my project tests?

Here are Contact:

3BD518FF8191FE1FC38073C821100A

and Contactless ATRs:

3B8580018073C821100E

and this is the ATR of a card which tested to work successfully with the same applet and APDU commands:

3B9B96803FC7A08031E073FE211B4B4522203F

Thanks in advance,

0 Kudos
Reply
3 Replies

3,398 Views
wayne3
Contributor I

I need the answer also, can any expert give some hints?

0 Kudos
Reply

3,547 Views
AlbertEin
Contributor I

Is there any NXP smartcard expert to answer me?

0 Kudos
Reply

3,358 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @AlbertEin ,

 

This product is not a mass market product supported here, you have to get in touch with NXP to sign an NDA for that and get in touch with NXP representative in GC or in Asia by summiting a private ticket.

 

How to request NDA online: 

Kan_Li_0-1692926641231.pngKan_Li_0-1692926641231.png

 

How to summit a private ticket:

https://www.nxp.com/video/tutorial-for-nxp-support-case-portal:NCP-VIDEO 

 

Hope that makes sense,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
Reply