NX5DV330

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NX5DV330

871件の閲覧回数
vsabino
Contributor I

Hi, I'm having issues with this chip.

Found odd behavior of the NXP switch, the output voltage is 1V less than the input if the load is Hi-Z.

Also found that the output voltage gets limited to 3.5V with constant load and increasing voltage.

I read in the datasheet that the Input and output voltages can be 0 to 5.5V, so why am I experiencing this limiting?

Thanks,
Victor

タグ(1)
0 件の賞賛
返信
0 返答(返信)