NVT2002DP(TSSOP)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NVT2002DP(TSSOP)

1,942件の閲覧回数
songgoon
Contributor I

Hello. I recently purchased 30 NVT2002DP level shifters and left a message because I was curious about how to use them.

I'm analyzing data sheets, and I wonder if pins 3 and 4 and 5 and 6 have differences in motion, or if we can simply use the same thing as having two signal paths.

To add explanation, I wonder if pin 3 (A1) and pin 4 (A2) can be used as independent level shift inputs/outputs, or if there is a dependent relationship between the two.

Thank you.

0 件の賞賛
返信
3 返答(返信)

1,934件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Songgoon,

please refer to figure 1. in the NVT2002 datasheet. The A1 and A2 can be used independently. Only dependence is between the A1, A2, B1, B2 and the EN pin. If the pin is held low, the four pins are in high impedance state. 

JozefKozon_0-1633087314521.pngJozefKozon_0-1633087314521.png

JozefKozon_1-1633087346556.pngJozefKozon_1-1633087346556.png

With Best Regards,

Jozef

1,932件の閲覧回数
songgoon
Contributor I

Thank you!

0 件の賞賛
返信

1,929件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Songgoon,

you welcome.

With Best Regards,

Jozef

0 件の賞賛
返信