NVT2002DP(TSSOP)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NVT2002DP(TSSOP)

1,965 次查看
songgoon
Contributor I

Hello. I recently purchased 30 NVT2002DP level shifters and left a message because I was curious about how to use them.

I'm analyzing data sheets, and I wonder if pins 3 and 4 and 5 and 6 have differences in motion, or if we can simply use the same thing as having two signal paths.

To add explanation, I wonder if pin 3 (A1) and pin 4 (A2) can be used as independent level shift inputs/outputs, or if there is a dependent relationship between the two.

Thank you.

0 项奖励
回复
3 回复数

1,957 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Songgoon,

please refer to figure 1. in the NVT2002 datasheet. The A1 and A2 can be used independently. Only dependence is between the A1, A2, B1, B2 and the EN pin. If the pin is held low, the four pins are in high impedance state. 

JozefKozon_0-1633087314521.png

JozefKozon_1-1633087346556.png

With Best Regards,

Jozef

1,955 次查看
songgoon
Contributor I

Thank you!

0 项奖励
回复

1,952 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Songgoon,

you welcome.

With Best Regards,

Jozef

0 项奖励
回复