NHS 3152

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NHS 3152

770件の閲覧回数
HafizUsman
Contributor I

Hi, Daniel,

I already discussed an issue regarding a project for the measurement of resistance/current using NHS3152 board with MCUxpressolink prob in the post mentioned below. 

https://community.nxp.com/t5/MCUXpresso-IDE/NHS3152/m-p/2090322/emcs_t/S2h8ZW1haWx8bWVudGlvbl9zdWJzY...

I am thankful for your guidance to complete the program (that is working now) to measure the current/resistance of connected resistor across (an01 to an04). Program is in the attached file. 

Through this I can get the I2D current value as  a single integer.

But now I am interested to take (extract) the multiple measurements of the same I2D (current value) like in the case of tlogger program (in SDK) where we just set the configuration and tap the mobile with a different NXP app (TLogger)  and it saves different temperature measured values (with a defined time gap) in the chip and the app (TLogger) reads the all measured values from the memory of chip.

I look forward for the guidance to upgrade the code for the above required application.

Regards,

HAFIZ

0 件の賞賛
返信
1 返信

729件の閲覧回数
Daniel_Gutierrez
NXP Employee
NXP Employee

Hello @HafizUsman, Good Day!

 

Unfortunately, sharing specific code implementations is out of our support scope.

 

However, if the purpose of your application is to send the calculated I2D value via an NDEF message to a tag reader as it is done in the app_demo_dp_tlogger example, I would suggest taking that example as a starting point in order to minimize modifications.

 

This application waits for an NDEF message containing a MIME record to arrive, it then extracts the payload and sends it to the "msg" module to generate a response, which is wrapped again in a message containing a single MIME record and written to the NFC memory for it to be retrieved by the reader.

 

A plausible option would be to replace the payload sent to the msg module with the result of the I2D conversion. The process of receiving and sending the payload to the msg module takes place in the "Execute(PMU_DPD_WAKEUPREASON_T wakeupReason)" function, found in maintlogger.c

 

I would suggest first running the example as it is to get a deeper understanding of its functionality and then implementing the code related to the I2D conversion. Please refer to the readme file of the example for further details about the application.

 

My best regards,
Daniel

0 件の賞賛
返信