NFC Cockpit Application

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NFC Cockpit Application

1,579件の閲覧回数
amighri
Contributor II

I wanted to ask why in the window of the NFC Cockpit Application on top between brackets 8disconnected9 thought I did the USB connection with the PNEV7462C card but App didn’t automatically read the board in the Guide supposed to be directly. Is there something I should do before ?

タグ(1)
0 件の賞賛
返信
1 返信

1,572件の閲覧回数
Fabian_R
NXP TechSupport
NXP TechSupport

Hello! Thank you for posting your question here.
In UM10883, section 6. After the NFC Cockpit installation, please mind that in sub-section 6.3. NFC Cockpit requires dedicated firmware to be running in the PN7462. This binary file is available in the NFC Cockpit installation and located in “<installation directory>\firmware\PN7462AU”.

Best Regards,
Fabian
0 件の賞賛
返信