Multiple SC18IM700 on same bus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multiple SC18IM700 on same bus

1,680件の閲覧回数
j_otisk
Contributor I

Hello,

I was unable to find if is possible to use multiple SC18IM700 on same bus and address each individualy to use theirs GPIO. It should work when using them as UART/I2C bridge because only valie i2c device will respond but how to address each SC18IM700 individually?

Thank you.

0 件の賞賛
返信
2 返答(返信)

1,558件の閲覧回数
lisettelozano
NXP Employee
NXP Employee

Hello,

First of all, please accept our apologies for the delayed response.

For this kind of application, the SC16IS752 can work as well.

Have a great day,

Paulina

0 件の賞賛
返信

1,558件の閲覧回数
j_otisk
Contributor I

Dear Paulina,

thank you for response, but SC16IS752 will not work in my application according to its datasheet it says i2c is SLAVE only.

I need to control I2C ADC through RS485 bus. So I designed following design:

MCU > RS485 > SC18IM700 as I2C master > I2C > ads1115 ADC

Idea is to build dumb ADC nodes on RS485 bus (nodes without MCU).

Question was if this will work with more SC18IM700 on bus because I cannot see any facility to address each of them separately. If all will receive packets and convert them to I2C them I'm ok too, because I2c is addressed so I can filter traffic on I2C slaves by their addresses.

0 件の賞賛
返信