Max speed for Multilink FX?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Max speed for Multilink FX?

1,109件の閲覧回数
tsweeney
Contributor I

Has anyone quantified the maximum speed for the Multilink FX emulator pod?  I can't find any information on NXP's or PE Micro's websites.  The only information I can find is that it is up to 10x faster than the Multilink Universal.

Connecting the pod to a Kinetis MCU the fastest speed I can get to reliably work for boundary scan and JTAG is 5MHz.  I would like to know if this is a limitation of my design or the Multilink FX.

0 件の賞賛
返信
1 返信

1,096件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, please contact PeMicro support

http://www.pemicro.com/support/index.cfm

as probably only they can answer the question correctly.

 

However maybe following thread on their forum could be helpful:

http://www.pemicro.com/forums/forum.cfm?forum_topic_id=6959

 

0 件の賞賛
返信