MSDI Inputs as Outputs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MSDI Inputs as Outputs

ソリューションへジャンプ
2,003件の閲覧回数
mark512
Contributor I

This is regarding the Multi Switch Detector Interface ICs.

On the datasheets for the MC33972, MC33975, MC34972 and MC34975, it's shown how the input wetting current supplies can be used like outputs to drive a small load like an LED.

On the datasheets for the MC33978, MC34978, CD1020 and CD1030, this application is not mentioned, but at a first glance it seems that there is no reason why these ICs wouldn't be able to do this as well. Is someone able to confirm that this works on these ICs too?

Thanks in advance!

0 件の賞賛
返信
1 解決策
1,990件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

No problem for them( MC33978, MC34978, CD1020 and CD1030) to drive LED. 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,991件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

No problem for them( MC33978, MC34978, CD1020 and CD1030) to drive LED. 

0 件の賞賛
返信